Maximum Number of Starts
The table lists the maximum number of starts for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0EB6 |
3767 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
|
1 |
Y |
Function setting |
|
0x0EB7 |
3768 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
1–30 |
6 |
Y |
Permissive starts |
|
0x0EB8 |
3769 |
1 |
0x03, |
RW |
1 |
min |
UINT16 |
15–60 |
30 |
Y |
Reference time |
|
0x0EB9 |
3770 |
1 |
0x03, |
RW |
1 |
min |
UINT16 |
1–120 |
5 |
Y |
Inhibit period |
|
0x0EBA |
3771 |
1 |
0x03, |
RW |
1 |
min |
UINT16 |
0–120 |
0 |
Y |
Time between starts |
|
0x0EBB |
3772 |
2 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |