Digital Output Status
The table lists the digital output status for the Modbus RTU communication.
|
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|
|
0x0020 |
33 |
0x02 |
R |
BOOL |
N |
Digital output 1 |
|
0x0021 |
34 |
0x02 |
R |
BOOL |
N |
Digital output 2 |
|
0x0022 |
35 |
0x02 |
R |
BOOL |
N |
Digital output 3 |
|
0x0023 |
36 |
0x02 |
R |
BOOL |
N |
Digital output 4 |
|
0x0024 |
37 |
0x02 |
R |
BOOL |
N |
Digital output 5 |
|
0x0025 |
38 |
0x02 |
R |
BOOL |
N |
Digital output 6 |
|
0x0026 |
39 |
0x02 |
R |
BOOL |
N |
Digital output 7 |
|
0x0027 |
40 |
0x02 |
R |
BOOL |
N |
Digital output 8 |
|
0x0028 |
41 |
0x02 |
R |
BOOL |
N |
Digital output 9 |
|
0x0029 |
42 |
0x02 |
R |
BOOL |
N |
Digital output 10 |
|
0x002A |
43 |
0x02 |
R |
BOOL |
N |
Digital output 11 |
|
0x002B |
44 |
0x02 |
R |
BOOL |
N |
Digital output 12 |
|
0x002C |
45 |
0x02 |
R |
BOOL |
N |
Digital output 13 |
|
0x002D–0x003F |
46–64 |
– |
– |
– |
– |
Reserved |