BITMAP Representation of Boolean Data
The boolean data can also be mapped using bitwise data. For example, the Digital Input Status is mapped bitwise in the following table.
|
BITMAP register |
BITMAP function code |
Boolean register |
Boolean function code |
Description |
|---|---|---|---|---|
|
5627.0 |
0x03 |
1 |
0x02 |
Digital Input 1 |
|
5627.1 |
0x03 |
2 |
0x02 |
Digital Input 2 |
|
5627.2 |
0x03 |
3 |
0x02 |
Digital Input 3 |
|
5627.3 |
0x03 |
4 |
0x02 |
Digital Input 4 |
|
5627.4 |
0x03 |
5 |
0x02 |
Digital Input 5 |
|
5627.5 |
0x03 |
6 |
0x02 |
Digital Input 6 |
|
5627.6 |
0x03 |
7 |
0x02 |
Digital Input 7 |
|
5627.7 |
0x03 |
8 |
0x02 |
Digital Input 8 |
|
5627.8 |
0x03 |
9 |
0x02 |
Digital Input 9 |
|
5627.9 |
0x03 |
10 |
0x02 |
Digital Input 10 |
|
5627.10 |
0x03 |
11 |
0x02 |
Digital Input 11 |
|
5627.11 |
0x03 |
12 |
0x02 |
Digital Input 12 |
|
5627.12 |
0x03 |
13 |
0x02 |
Digital Input 13 |
|
5627.13 |
0x03 |
14 |
0x02 |
Digital Input 14 |
|
5627.14 |
0x03 |
15 |
0x02 |
Digital Input 15 |
|
5627.15 |
0x03 |
16 |
0x02 |
Digital Input 16 |
|
5626.0 |
0x03 |
17 |
0x02 |
Digital Input 17 |
|
5626.1 |
0x03 |
18 |
0x02 |
Digital Input 18 |
|
5626.2 |
0x03 |
19 |
0x02 |
Digital Input 19 |
|
5626.3 |
0x03 |
20 |
0x02 |
Digital Input 20 |
|
5626.4 |
0x03 |
21 |
0x02 |
Digital Input 21 |
|
5626.5 |
0x03 |
22 |
0x02 |
Digital Input 22 |
|
5626.6 |
0x03 |
23 |
0x02 |
Digital Input 23 |
|
5626.7 |
0x03 |
24 |
0x02 |
Digital Input 24 |