DOCA0355EN-01

Thermal Overload Protection

The table lists the thermal overload protection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0DAC

3501

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm + Trip

3

Y

Function setting

0x0DAD

3502

1

0x03,
0x06,
0x10

RW

0.01

UINT16

100–150
(step 5)

115

Y

Service factor

0x0DAE

3503

1

0x03,
0x06,
0x10

RW

1

UINT16

5–40
(step 5)

10

Y

Trip class

0x0DAF

3504

1

0x03,
0x06,
0x10

RW

1

%TM*

UINT16

80–100
(step 5)

80

Y

Alarm level

0x0DB0

3505

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

8

Y

Reset mode*

0x0DB1

3506

1

0x03,
0x06,
0x10

RW

1

%TM*

UINT16

30–95
(step 5)

90

Y

Thermal reset level

0x0DB2

3507

1

0x03,
0x06,
0x10

RW

1

%TM*

UINT16

5–100
(step 5)

90

Y

Start inhibit level

0x0DB3

3508

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Cool down function

0x0DB4

3509

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Cool down time

0x0DB5

3510

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Pause function

0x0DB6

3511

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Pause time

0x0DB7

3512

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Block function

0x0DB8

3513

1

0x03,
0x06,
0x10

RW

1

%TM*

UINT16

80–95
(step 5)

80

Y

Block level

0x0DB9

3514

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Block time

0x0DBA

3515

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Auxiliary fan

0x0DBB

3516

3

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?