Statistic Data
The table lists the statistic data for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x1676 |
5751 |
1 |
0x03 |
R |
1 |
ms |
UINT16 |
N |
Timer 1 - Actual value |
|
0x1677 |
5752 |
1 |
0x03 |
R |
1 |
ms |
UINT16 |
N |
Timer 2 - Actual value |
|
0x1678 |
5753 |
1 |
0x03 |
R |
1 |
ms |
UINT16 |
N |
Timer 3 - Actual value |
|
0x1679 |
5754 |
1 |
0x03 |
R |
1 |
ms |
UINT16 |
N |
Timer 4 - Actual value |
|
0x167A |
5755 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Counter 1 - Actual value |
|
0x167B |
5756 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Counter 2 - Actual value |
|
0x167C |
5757 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Counter 3 - Actual value |
|
0x167D |
5758 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Counter 4 - Actual value |
|
0x167E |
5759 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Thermal overload trip counter |
|
0x167F |
5760 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Locked rotor trip counter |
|
0x1680 |
5761 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Stalled rotor trip counter |
|
0x1681 |
5762 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Definite time overcurrent trip counter |
|
0x1682 |
5763 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Normal inverse overcurrent trip counter |
|
0x1683 |
5764 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Short time overcurrent trip counter |
|
0x1684 |
5765 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Calculated ground trip counter |
|
0x1685 |
5766 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Measured ground trip counter |
|
0x1686 |
5767 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Phase under current trip counter |
|
0x1687 |
5768 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Current imbalance trip counter |
|
0x1688 |
5769 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Current phase loss trip counter |
|
0x1689 |
5770 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Current phase reversal trip counter |
|
0x168A |
5771 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Phase under voltage trip counter |
|
0x168B |
5772 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Phase over voltage trip counter |
|
0x168C |
5773 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Voltage phase loss trip counter |
|
0x168D |
5774 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Voltage imbalance trip counter |
|
0x168E |
5775 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Voltage phase reversal trip counter |
|
0x168F |
5776 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Under frequency trip counter |
|
0x1690 |
5777 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Over frequency trip counter |
|
0x1691 |
5778 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Excessive start time trip counter |
|
0x1692 |
5779 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Communication loss trip counter |
|
0x1693 |
5780 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
LTMT main unit temperature trip counter |
|
0x1694 |
5781 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Under power trip counter |
|
0x1695 |
5782 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Over power trip counter |
|
0x1696 |
5783 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Under power factor trip counter |
|
0x1697 |
5784 |
1 |
– |
– |
– |
– |
– |
– |
Reserved |
|
0x1698 |
5785 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Device internal trip counter |
|
0x1699 |
5786 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
HMI communication loss trip counter |
|
0x169A–0x169D |
5787 – 5790 |
1 |
– |
– |
– |
– |
– |
– |
Reserved |
|
0x169E |
5791 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 1 trip counter |
|
0x169F |
5792 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 2 trip counter |
|
0x16A0 |
5793 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 3 trip counter |
|
0x16A1 |
5794 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 4 trip counter |
|
0x16A2 |
5795 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 5 trip counter |
|
0x16A3 |
5796 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 6 trip counter |
|
0x16A4 |
5797 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 7 trip counter |
|
0x16A5 |
5798 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 8 trip counter |
|
0x16A6 |
5799 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 9 trip counter |
|
0x16A7 |
5800 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 10 trip counter |
|
0x16A8 |
5801 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 11 trip counter |
|
0x16A9 |
5802 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
DI interlock 12 trip counter |
|
0x16AA |
5803 |
1 |
– |
– |
– |
– |
– |
– |
Reserved |
|
0x16AF–0x16C1 |
5807–5822 |
1 |
– |
– |
– |
– |
– |
– |
Reserved |
|
0x16BE |
5823 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Analog input 1 trip counter |
|
0x16BF |
5824 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Analog input 2 trip counter |
|
0x16C0 |
5825 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Analog input 3 trip counter |
|
0x16C1 |
5826 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Analog input 4 trip counter |
|
0x16C2 |
5827 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Analog 1 output @Updated D5
|
|
0x16C3 |
5828 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Analog 2 output @Updated D5
|
|
0x16C4 |
5829 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Motor stop error detection trip counter |
|
0x16C5 |
5830 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Logic test interrupted trip counter |
|
0x16C6 |
5831 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Stucked reset key trip counter |