Hysteresis Settings
The table lists the registers for the hysteresis settings.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x109A |
4251 |
1 |
0x03, |
RW |
1 |
% |
UINT16 |
3–15 (step 1) |
3 |
Y |
Current protection |
|
0x109B |
4252 |
1 |
0x03, |
RW |
1 |
% |
UINT16 |
3–15 (step 1) |
3 |
Y |
Voltage protection |
|
0x109C |
4253 |
1 |
0x03, |
RW |
1 |
% |
UINT16 |
1–15 (step 1) |
3 |
Y |
Frequency protection |
|
0x109D |
4254 |
1 |
0x03, |
RW |
1 |
% |
UINT16 |
3–15 (step 1) |
3 |
Y |
Power protection |
|
0x109E |
4255 |
1 |
0x03, |
RW |
1 |
mA |
UINT16 |
1–3 |
1 |
Y |
Analog input protection |
|
0x109E–0x109F |
4256 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |