Motor Data
The table lists the motor data for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x15B5 |
5558 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Motor status
|
|
0x15B6 |
5559 |
1 |
0x03 |
R |
1 |
% |
UINT16 |
Y |
Thermal memory |
|
0x15B7 |
5560 |
2 |
0x03 |
R |
1 |
s |
UINT32 |
N |
Thermal time to trip |
|
0x15B9 |
5562 |
2 |
0x03 |
R |
1 |
s |
UINT32 |
N |
Thermal time to cool |
|
0x15BB |
5564 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
Y |
Max starts counter or Max starts per hour counter |
|
0x15BC |
5565 |
2 |
0x03 |
R |
1 |
s |
UINT32 |
Y |
Max start time or Max start inhibit time |
|
0x15BE |
5567 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
N |
Motor starting peak current |
|
0x15C0 |
5569 |
2 |
0x03 |
R |
0.001 |
s |
UINT32 |
N |
Motor starting time |
|
0x15C2 |
5571 |
2 |
0x03 |
R |
1 |
min |
UINT32 |
Y |
Total run hour |
|
0x15C4 |
5573 |
2 |
0x03 |
R |
1 |
min |
UINT32 |
Y |
Last run hour |
|
0x15C6 |
5575 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
Y |
Number of starts |
|
0x15C7 |
5576 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
Y |
Number of stops |
|
0x15C8 |
5577 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
Y |
Motor stop cause
|
|
0x15C9 |
5578 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
Y |
Trip counter |