Under Power Protection
The table lists the under power protection for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0E57 |
3672 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0E58 |
3673 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%P * |
UINT16 |
20–1000 |
60 |
Y |
Pickup |
|
0x0E59 |
3674 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
|
0x0E5A |
3675 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%P * |
UINT16 |
20–1000 |
60 |
Y |
Alarm level |
|
0x0E5B |
3676 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0E5C |
3677 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E5D |
3678 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |