DOCA0355EN-01

Modbus RTU Settings

The table lists the Modbus RTU settings for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X Unit

Type

Range Default value

Svd

Description

0x1129

4394

1

0x03,
0x10

RW

1

UINT16

1–247
(step 1)

1

Y

Node address

0x112A

4395

1

0x03,
0x10

RW

1

UINT16

0: None

1: Odd

2: Even

2

Y

Parity

0x112B

4396

1

0x03,
0x10

RW

1

bps

UINT16

0: 2400

1: 4800

2: 9600

3: 19200

4: 38400

5: 57600

6: 115200

3

Y

Baud rate

0x112C

4397

1

Reserved

0x112D

4398

1

0x03,
0x10

RW

1

s

UINT16

1–60000
(step 1)

1

Y

Timeout*

0x112E

4399

1

0x03,
0x10

RW

BITMAP

0: Big-endian

1: Little-endian

0

Y

Byte format

The TeSys Tera system detects communication loss or timeout after the timeout period. A time delay is implemented following the detection of communication loss or timeout.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?