Bus Coupler LEDs
TPRBCEIP EtherNet/IP™ Bus Coupler LEDs
|
LED |
Color |
State |
Description |
|---|---|---|---|
|
PWR |
Dual LED, Yellow/Green |
||
|
Yellow |
Static |
System is booting. |
|
|
Green |
On |
Operating system running. |
|
|
Off |
Off |
Power supply for the device is missing, or hardware is not operational. |
|
|
Yellow |
Static (5 s) |
Identification of the connected bus coupler following a Locate command. Other LED behavior is overridden for 5 s. |
|
|
Yellow |
Flashing |
System is in Force Mode. |
|
|
MS Name in the device drawing: COM 0 |
Dual LED, Red/Green |
||
|
Green |
On |
Device operational: The device is operating correctly. |
|
|
Green |
Flashing |
Standby: The device has not been configured. |
|
|
Red |
On |
Major event: The device has detected a non-recoverable major event. |
|
|
Red |
Flashing |
Minor event: The device has detected a recoverable minor event. NOTE: An incorrect or inconsistent configuration is a minor event.
|
|
|
Red/Green |
Flashing |
Self-test: The device is performing its power-up testing. |
|
|
Off |
Off |
No power: No power is supplied to the device. |
|
|
NS Name in the device drawing: COM 1 |
Dual LED, Red/Green |
||
|
Green |
On |
Connected: The device has at least one established connection (even to the message router). |
|
|
Green |
Flashing |
No connections: The device has no established connections but has obtained an IP address. |
|
|
Red |
On |
Duplicate IP: The device has detected that its IP address is already in use. |
|
|
Red |
Flashing |
Connection timeout: One or more of the connections targeting this device has timed out. This condition is cleared only if all timed out connections are reestablished or if the device is reset. |
|
|
Red/Green |
Flashing |
Self-test: The device is performing its power-up testing. |
|
|
Off |
Off |
Not powered, no IP address: The device does not have an IP address, or is powered off. |
|
|
LINK/RJ45 ETH and TER Ports |
LED, Green |
||
|
Green |
On |
The device is connected to the Ethernet network. |
|
|
Off |
Off |
The device is not connected to the Ethernet network. |
|
|
ACT/RJ45 ETH and TER Ports |
LED, Yellow |
||
|
Yellow |
Flashing |
The device is sending or receiving Ethernet frames. |
|
|
BS/ERR |
Black |
Off |
No connection to internal bus. |
|
Blinking green |
On with COM |
Connection / communication to internal bus. |
|
|
Steady green |
On |
Connection to internal bus. |
|
TPRBCPFN PROFINET® Bus Coupler LEDs
|
LED |
Color |
State |
Description |
|---|---|---|---|
|
PWR |
Dual LED, Yellow/Green |
||
|
Yellow |
Static |
System is booting. |
|
|
Green |
On |
Operating system is running. |
|
|
Green |
Flashing (3 s) |
The bus coupler received a DCP signal command from the PROFINET network. |
|
|
Off |
Off |
The power supply for the device is missing, or the hardware is not operational. |
|
|
Yellow |
Static (5 s) |
Identification of the connected bus coupler following a Locate command. Other LED behavior is overridden for 5 s. |
|
|
Yellow |
Flashing |
The system is in Force mode. |
|
|
SF Name in the device drawing: COM 0 |
Dual LED, Red/Green |
||
|
Red |
On |
The system transitions to the status, Major Event State Active (problem indicator within a Diagnosis alarm). |
|
|
Red |
Flashing (3 s) |
The DCP service is being initiated. |
|
|
Off |
Off |
No system errors and no ongoing DCP configuration. |
|
|
BF Name in the device drawing: COM 1 |
Dual LED, Red/Green |
||
|
Red |
On |
No configuration; or low speed physical link; or no physical link. |
|
|
Red |
Flashing |
No data exchange. |
|
|
Off |
Off |
— |
|
|
LINK/RJ45 PFN and TER Ports |
LED, Green |
||
|
Green |
On |
The device is connected to the Ethernet network. |
|
|
Off |
Off |
The device is not connected to the Ethernet network. |
|
|
ACT/RJ45 PFN and TER Ports |
LED, Yellow |
||
|
Yellow |
Flashing |
The device is sending or receiving Ethernet frames. |
|
|
BS/ERR |
Black |
Off |
No connection to internal bus. |
|
Blinking green |
On with COM |
Connection / communication to internal bus. |
|
|
Steady green |
On |
Connection to internal bus. |
|
TPRBCPFB PROFIBUS® Bus Coupler LEDs
|
LED |
Color |
State |
Description |
|---|---|---|---|
|
PWR |
Dual LED, Yellow/Green |
||
|
Yellow |
Static |
System is booting. |
|
|
Green |
On |
Operating system is running. |
|
|
Off |
Off |
Power supply for the device is missing, or hardware is not operational. |
|
|
Yellow |
Static (5 s) |
Identification of the connected bus coupler following a Locate command. Other LED behavior is overridden for 5 s. |
|
|
Yellow |
Flashing |
The system is in Force mode. |
|
|
MS Name in the device drawing: COM 0 |
Dual LED, Red/Green |
||
|
Green |
On |
Device operational: The device is operating correctly. |
|
|
Green |
Flashing |
Standby: The device has not been configured. |
|
|
Red |
On |
Major event: The device has detected a non-recoverable major event. |
|
|
Red |
Flashing |
Minor event: The device has detected a recoverable minor event. NOTE: An incorrect or inconsistent
configuration is a minor event.
|
|
|
Red/Green |
Flashing |
Self-test: The device is performing its power-up testing. |
|
|
Off |
Off |
No power: No power is supplied to the device. |
|
|
COM Name in the device drawing: COM 1 |
Dual LED, Red/Green |
||
|
Green |
On |
Cyclic communication. |
|
|
Red |
Flashing (cyclic) |
No communication—connection error. |
|
|
Red |
Flashing (acyclic) |
Not configured. |
|
|
Off |
Off |
— |
|
|
LINK/RJ45 TER Port |
LED, Green |
||
|
Green |
On |
The device is connected to the Ethernet network. |
|
|
Off |
Off |
The device is not connected to the Ethernet network. |
|
|
ACT/RJ45 TER Port |
LED, Yellow |
||
|
Yellow |
Flashing |
The device is sending or receiving Ethernet frames. |
|
|
BS/ERR |
Black |
Off |
No connection to internal bus. |
|
Blinking green |
On with COM |
Connection / communication to internal bus. |
|
|
Steady green |
On |
Connection to internal bus. |
|
Visual LED for SD Card
|
LED color status (Green/Red) |
System status |
Description |
|---|---|---|
|
Steady Off |
None |
System power is off. |
|
Green, Steady On |
Normal |
Data files on the memory card used for FDR are identical with data files on the device. |
|
Green, Blinking |
Data exchanges |
Read data from the SD card or write data on the SD card. |
|
Red, Blinking |
Alarm—SD Card Event |
Data files on the memory card used for FDR are not identical with data on the device after update. SD card cannot be read or written, or SD card is missing. |
|
Red, Steady On |
Minor event |
2 project files on the SD card. |