Performing a Factory Reset
The TeSys island system can be reset to factory settings, returning the bus coupler to its out-of-the-box conditions. This is useful, for example, to quickly get to Test mode when building or modifying an island.
TeSys island accepts a Factory Reset command from the digital tool (TeSys island DTM or OMT) with exclusive control when the system is in Pre-Operational mode, Test mode, or Minor Event state.
Upon receiving a Factory Reset command, TeSys island
-
Deletes the following files:
-
system context files (active, pending, and SDP if present)
-
SEDP files (including active, pending, or update)
-
Users file
-
-
Automatically restarts
-
When the Users file is deleted, any added users are removed. In addition, the group management and the administrative password are reset to default values.
-
A Factory Reset command does not delete log files.
Using the TeSys island DTM
To perform a factory reset using the TeSys island DTM, follow the steps below:
-
In the TeSys island DTM, select Device > Factory Reset.
-
Click OK to perform the factory reset.
-
The island starts the reset procedure.
-
The PWR LED on the bus coupler is yellow.
-
The LEDs on the rest of the modules flash green.
-
Using the TeSys island OMT
To perform a factory reset using the OMT, follow the steps below:
-
Click the Admin Options panel.
-
Expand the System Settings section.
-
Click the Restore Factory Defaults button.
-
Click OK to continue with the factory reset.
-
The island starts the reset procedure.
-
The PWR LED on the bus coupler is yellow.
-
The LEDs on the rest of the modules flash green.