Micro SD Card
Use this option to replace the bus coupler if there is a micro SD card installed in the existing bus coupler.
Prerequisite: This option is valid only to replace a bus coupler which has stored data on a micro SD Card (that is, the SD Card visual indicator on the Bus Coupler being replaced has been in the Green, Steady On state).
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Turn off all power before working on or inside the equipment.
Failure to follow these instructions will result in death or serious injury.
|
-
Disconnect all power from the island.
-
Remove the micro SD card from the existing bus coupler.
-
Insert the micro SD card into the replacement bus coupler.
-
Remove the existing bus coupler from the DIN rail and install the replacement module by following the instructions in Installing the Bus Coupler in the TeSys island Installation Guide.
-
Apply power to the island, initiating the boot process. Observe the LEDs on the bus coupler until they turn green, indicating that the island has entered the operating state. The boot process takes about two minutes.
DANGER