DOCA0270EN-02

Starters and Power Interface Modules

To view the device status, click one of the starters or power interface modules in the island view. This action opens a new window displaying the status of the device. The following information is provided:

  • Device Status

    • Name tag

    • Position

    • Commercial reference number

    • Status

    • Irms

    • Upstream voltage presence

  • Asset Data

    • Number of device power cycles

    • Time device on

    • Number of device events

    • Time switch on (starter only)

    • Number of contactor cycles (starter only)

    • Maximum RMS current

    • Lifetime average RMS current

  • Product Identification

    • Vendor name

    • Vendor URL

    • Model name

    • Serial number

    • Firmware version

    • Product code

  • Device Logs

  • Test Command

Island View: Devices

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?