SoMove™ Project File
Use this option to replace the bus coupler when a working micro SD card is not available, and FDR is not an option.
Prerequisite: A SoMove project file can be loaded onto the replacement bus coupler using the TeSys island DTM.
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or Arc Flash
Turn off all power before working on or inside the equipment.
Failure to follow these instructions will result in death or serious injury.
|
-
Disconnect all power from the island.
-
Remove the micro SD card from the existing bus coupler if one is installed.
-
Set the micro SD card aside. Do not insert the micro SD card into the replacement bus coupler.
-
Remove the existing bus coupler from the DIN rail and install the replacement module by following the instructions in “Installing the Bus Coupler” in the TeSys™ island Installation Guide.
-
Apply power to the island, initiating the boot process. Observe the LEDs until they turn green, indicating that the island has entered the operating state. The boot process takes about two minutes.
-
Connect to the island via the TeSys island DTM, and load the SoMove project file as follows:
-
Launch the TeSys island DTM.
-
Connect to the island.
-
Click Store to Device.
-
Select the project file that you wish to load from the PC to the bus coupler.
NOTE: The TeSys island DTM triggers the island to reboot as part of the process of loading the project file. Observe the LEDs until they turn green, indicating that the island has entered the operating state. The boot process takes about two minutes.
-
DANGER