DOCA0270EN-02

Conveyor Two Directions - SIL Stop, W. Cat 1/2

Safety Integrity Level according to standard IEC 61508. Wiring Category 1 and Category 2 according to ISO 13849.

Wiring (See Legend Table below)

NOTE: Analog I/O modules (AIOMs) and digital I/O modules (DIOMs) are configurable.

Accessories

Legend

A Mechanical interlock
B Parallel link
C Reversing link
F Forward
R Reverse
SS-1 SIL starter 1
SS-2 SIL starter 2

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?