DOCA0270EN-02

Motor Two Speeds - SIL Stop, W. Cat 1/2

NOTE: Safety Integrity Level according to standard IEC 61508. Wiring Category 1 and Category 2 according to ISO 13849.

Low Speed Wiring

Accessories

Legend

A

Mechanical interlock

B

Parallel link

LS

Low speed

HS

High speed

SS-1

SIL starter 1

SS-2

SIL starter 2

High Speed Wiring

Accessories

Legend

A

Mechanical interlock

B

Parallel link

LS

Low speed

HS

High speed

SS-1

SIL starter 1

SS-2

SIL starter 2

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?