Protection Functions
TeSys island offers a wide range of load protection functions (including thermal protection) and electrical protection functions. These functions can be enabled for each applicable TeSys avatar, and configured to react to given operational conditions, by signaling alarm messages and triggering load trips.
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Make sure to set the protection functions parameters according
to the required protection level of the controlled motors and loads.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The following table lists the protection functions available for all avatars . The functions can be enabled and configured individually.
Protection Functions
|
Load Protection Functions |
Thermal Protection Functions |
|---|---|
|
|
|
Electrical Protection Functions |
|
|
The following table defines parameters that are associated with multiple protection functions. They are referred to throughout the protection function sections in this guide.
Common Protection Function Parameters
|
Parameter |
Definition |
|---|---|
|
<function name> Trip Enable |
Enables the trip function |
|
<function name> Trip Delay |
A time setting specifying the duration that a trip condition must exist to trigger a trip |
|
<function name> Trip Level |
A setting to define the level of an input that triggers a trip |
|
<function name> Alarm Enable |
Enables the alarm function |
|
<function name> Alarm Level |
A setting to define the level of an input that triggers an alarm |
WARNING