DOCA0270EN-02

Installation Verification

Once you have mounted all TeSys island modules on the DIN rail, using the TeSys island topology, verify that each module is in the proper location and sequence on the TeSys island . If any modules are incorrectly positioned on the TeSys island , remove the modules from the DIN rail and install them in the proper location following the installation procedures.

Once you have verified that the modules are in the correct location, install a type ABB8P35 or equivalent terminal block end clamp (A)

  • to the left of the bus coupler and to the right of the last module on the island if you are mounting the TeSys island horizontally, or

  • below the bus coupler and above the last module on the TeSys island if you are mounting the TeSys island vertically.

End clamps help minimize movement and improve the shock and vibration characteristics of the TeSys island .

End Clamp in Horizontal Orientation

End Clamp in Vertical Orientation

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?