DOCA0270EN-02

Change Password

To change your OMT password once logged into the OMT, perform the following steps:

  1. Click the Hello link (user link) at the top of the main OMT panel.

    Result: The USER PREFERENCES and ACCOUNT SETTINGS window opens.

    User Preferences

  2. In the ACCOUNT SETTINGS section, click Change Password.

  3. Enter the current password.

  4. Enter the new password twice.

  5. Click Submit.

NOTE: Passwords must contain a minimum of 10 characters, with at least one alphabetic and one numeric character.

Change Password

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?