Thermal Considerations
The following tables list maximum thermal dissipation values for planning your TeSys island cooling system. The values assume maximum bus voltage, maximum field-side voltage, and maximum load currents. Typical values are often lower.
Maximum Thermal Dissipation Values: Starters and Power Interface Modules
|
Module Type |
Reference Number |
Maximum Thermal Dissipation @ AC3 |
Maximum Thermal Dissipation @ AC1 |
|---|---|---|---|
|
Standard Starters |
TPRST009 |
3.5 |
5.1 |
|
TPRST025 |
6.6 |
8.3 |
|
|
TPRST038 |
11.8 |
12.8 |
|
|
TPRST065 |
20.3 |
30.5 |
|
|
TPRST080 |
30.5 |
30.5 |
|
|
SIL* Starters |
TPRSS009 |
3.5 |
5.1 |
|
TPRSS025 |
6.6 |
8.3 |
|
|
TPRSS038 |
11.8 |
12.8 |
|
|
TPRSS065 |
20.3 |
30.5 |
|
|
TPRSS080 |
30.5 |
30.5 |
|
|
Power Interface Modules |
TPRPM009 |
0.6 |
1.3 |
|
TPRPM038 |
0.9 |
1.0 |
|
|
TPRPM080 |
2.3 |
2.3 |
Maximum Thermal Dissipation Values: Bus Coupler, SIL Interface Module, Voltage Interface Module, I/O Modules
|
Module Type |
Reference Number |
Maximum Thermal Dissipation |
|---|---|---|
|
Bus Coupler |
TPRBCEIP |
5.00 |
|
TPRBCPFN |
5.00 |
|
|
TPRBCPFB |
5.00 |
|
|
SIL Interface Module |
TPRSM001 |
1.25 |
|
Voltage Interface Module |
TPRVM001 |
0.20 |
|
Digital I/O Module |
TPRDG4X2 |
1.20 |
|
Analog I/O Module |
TPRAN2X1 |
1.70 |