DOCA0270EN-02

IP Allowlist

IP Allowlist enables you to configure an Access Control List (ACL) of IP addresses that are allowed to communicate with the bus coupler.

To enable and set the IP Allowlist settings for the system, do the following:

  1. In the Admin Options panel, click the arrow to expand the IP Allowlist.

  2. Change the IP Allowlisting setting to Enable.

  3. Click the plus sign to add a new IP address.

  4. Enter the IP Address and Netmask.

  5. Click Save.

IP Allowlist

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?