Load Avatars
Standard (non-SIL*) load avatars include the following:
-
Standard starter modules
-
One or more digital I/O modules for PV switches and local control inputs
-
One or more analog I/O modules for PV inputs and motor temperature monitoring, if enabled
-
Configurable control logic is enabled for the avatar when the Local Control Enabled Avatar Parameter is set to Yes during the build phase.
The load avatars that include configurable control logic are as follows:
-
Motor One Direction
-
Motor Two Directions
-
Motor Y/D One Direction
-
Motor Y/D Two Directions
-
Motor Two Speeds
-
Motor Two Speeds Two Directions
-
Motor One Direction-SIL Stop, W. Cat 1/2
-
Motor One Direction-SIL Stop, W. Cat 3/4
-
Motor Two Directions-SIL Stop, W. Cat 1/2
-
Motor Two Directions-SIL Stop, W. Cat 3/4
-
Motor Two Speeds-SIL Stop, W .Cat 1/2
-
Motor Two Speeds-SIL Stop, W. Cat 3/4
-
Motor Two Speeds Two Directions-SIL Stop, W. Cat 1/2
-
Motor Two Speeds Two Directions-SIL Stop, W. Cat 3/4
-
Resistor
-
Power Supply
-
Transformer
-
Power Interface with IO