DOCA0270EN-02

OMT IPv4 Connection

Use this procedure to connect to TeSys™ island with the Operation and Maintenance Tool (OMT) after the island has been physically installed and powered up. If the TeSys island is set to DHCP (which is the default) then the OMT can connect directly to the bus coupler using the default IPv4 address.

To perform this procedure, the island must be on the network and able to communicate with the OMT using a wireless or wired connection.

Connecting to the TeSys island with the OMT via the default IPv4 address

  1. Verify that your PC is connected to the same network as the bus coupler through a wireless or wired connection.

  2. Configure your PC with the IPv4 IP address of 10.10.0.2 and the subnet mask of 255.0.0.0

  3. Enter the address (https://10.10.0.1) of the bus coupler into the web browser on your tablet to access the OMT running on the bus coupler.

    NOTE: The recommended browsers are Chrome or Safari.
  4. If you are taken to the page, "Your connection is not private":

    1. Click Advanced.

    2. Click the link "Proceed to 10.10.0.1 (unsafe)" to continue.

  5. Log in with the default username and password (admin, schneider18) and click Login.
    The Change Password window opens.

  6. Set a secure password and record it before continuing.

    NOTE: If you forget your password, a factory reset will be required to regain access to the OMT.

You are now logged in to the OMT and connected to the island.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?