DOCA0270EN-02

Technical Specifications

TeSys island Specifications

Width up to 112.5 cm (3.83 ft)
Modules up to 20 modules, excluding the bus coupler and the voltage interface modules
PROFIBUS fieldbus only: Cyclic data size limit Maximum size of 240 bytes possible
Control power consumption per system 3 A or 72 W maximum
Maximum load current per starter 80 A, 37 kW (50 hp), maximum
Internal data refresh time 10 ms
Mounting Metallic DIN rail, horizontal or vertical
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?