Force Mode
WARNING |
|---|
|
Unintended equipment operation
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Once the TeSys island is in the operational state, Force mode can be activated and deactivated using the OMT or TeSys island DTM.
Using Force Mode to Simulate Commands from the PLC
Force mode allows you to test the logic of any TeSys avatar by simulating receipt of commands from the PLC.
Simulating a PLC Command with Force Mode
|
Step |
Action |
|
1 |
Access Force mode:
|
|
2 |
To simulate receipt of a PLC command:
|
|
3 |
When finished, exit Force mode. See Exiting Force Mode. |
Using Force Mode to Simulate Status Updates to the PLC
Force mode also allows you to simulate transmission of avatar status updates from the island to the PLC.
Simulating Avatar Status Updates from the Island to the PLC
|
Step |
Action |
|
1 |
Access Force mode from the OMT or TeSys island DTM as described in Simulating a PLC Command with Force Mode. |
|
2 |
To simulate avatar status:
|
|
3 |
When finished, exit Force mode. See Exiting Force Mode. |
Using Force Mode to Simulate Status Changes of the Digital I/O Module Inputs and Outputs
Force mode also allows you to simulate status changes of the digital I/O module inputs and outputs. When force mode has not been applied, the status box is gray and shows Not Applied.
Status Box
| Force Command | Input From PLC | Status To PLC |
|---|---|---|
|
Force 0 |
Off |
Off |
|
Force 1 |
On |
On |
|
Step |
Action |
|
1 |
Access Force mode from the OMT or TeSys island DTM as described in Simulating a PLC Command with Force Mode. |
|
2 |
To simulate I/O status, under From PLC:
|
|
Under To PLC:
|
Exiting Force Mode
To exit Force mode, perform the steps in the following table:
Exiting Force Mode
|
Step |
Action |
|
|---|---|---|
|
1 |
To exit Force mode using the TeSys island DTM, in the Diagnostics tab, click Exit next to Force Mode, and then confirm you wish to exit. |
|
|
2 |
To exit Force mode from the OMT: |
|
|
Click the Diagnostics panel. |
||
|
Click the Exit force mode button. A hazard message pop-up window appears. Click Yes to confirm that you want to exit Force mode. The status banner at the top indicates that the system is no longer in Force mode. |
||
WARNING