Thermal Protection
Thermal protection settings values
| Setting Name | Value Range | Default Value | Increment |
|
Ir (FLA) |
|
|
0.01 |
|
Ir (FLA) 2 |
|
|
0.01 |
| Thermal Overload Trip Class |
5–30 |
10 |
— |
| Thermal Overload Reset Threshold |
10–95% |
85% |
1 |
| Thermal Overload Alarm Level |
10–100% |
85% |
1 |
| Motor Overheat Trip Delay |
0–10 s |
5 s |
0.1 |
| Motor Overheat Trip Level |
0–200 °C |
0 °C |
1 |
| Motor Overheat Reset Threshold |
0–200 °C |
0 °C |
1 |
| Motor Overheat Alarm Threshold |
0–200 °C |
0 °C |
1 |
| Motor Overheat Temperature Sensor |
|
PT 100 |
— |