DOCA0270EN-02

Overcurrent

TeSys avatars with Overcurrent Alarm enabled signal an Overcurrent Alarm if the maximum phase current exceeds the Overcurrent Alarm Level in the motor Run state.

Avatars with Overcurrent Trip enabled signal an Overcurrent Trip if the maximum phase current exceeds the Overcurrent Trip Level in the motor Run state for a time longer than the Overcurrent Trip Delay.

Overcurrent Trip and Alarm

I1

Phase 1 Current

I2

Phase 2 Current

I3

Phase 3 Current

A

Imax

B

Imax ≥ Overcurrent Alarm Level

C

Imax ≥ Overcurrent Trip Level

D

Run State

E

Overcurrent Alarm

F

Overcurrent Trip

T

Overcurrent Trip Delay

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?