DOCA0270EN-02

Alarm Input

There are two Alarm Inputs that can be set up for the avatar : Alarm Input 1 and Alarm Input 2. You can set up a unique type of input for each of these alarm inputs. The following inputs are available:

  • Temperature

  • Pressure

  • Flow

  • Vibration

  • Proximity

  • Generic

Each Predictive Alarm Input has the following two alarm threshold values that you can set:

  • Alarm High Threshold Value: Specifies the threshold between the low and nominal region of operation

  • Alarm Low Threshold Value: Specifies the threshold between the high and nominal regions of operation

Nominal is the region between the high and low threshold values. For example, if the high threshold value is set at 10 °C and the low threshold value is set at 2 °C, anything greater than 10 °C is considered high threshold values. Low threshold values are 0–2 °C. The nominal range is from 2–10 °C.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?