DOCA0270EN-02

Audit Log Format

  • TeSys island formats the timestamp in the Audit Log in the following format:

    YYYY-MM-DDThh:mm:ss.mmm

    Example: 2018-01-02T15:02:59.980

  • TeSys island formats the source in the Audit Log in the following format with valid values as defined below:

    <<source IP address>>,<<type of tool>>,<<user name>>

NOTE: If the source IP address is not known, a hyphen (-) is substituted.

Valid values for <<type of tool>> are

  • DTM

  • OMT

  • other

Valid values for <<user name>> are

  • the user name for the OMT tool type

  • a hyphen (-) for the DTM and the other tool type

Examples:

  • 192.168.100.1,OMT,Bob

  • 192.168.0.1,DTM,-

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?