DOCA0270EN-02

Counters

To access the trip and alarm counters for the TeSys avatar, click the Counters tab in the Avatar window.

Avatar Counters View

The following information is displayed for the avatar in the Counters view:

  • Trip Counters

  • Alarm Counters

  • Auto Reset Counters

  • Trip Record Register (last five trips)

To set the Trip or Alarm counters back to zero, click the Reset button.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?