DOCA0270EN-02

Mounting Power Interface Modules on DIN Rail

Before installing modules on the TeSys island , refer to the TeSys island topology to ensure you are installing them in the correct sequence.

To install a power interface module (PIM) on DIN rail, position the top groove of the PIM on the top edge of the DIN rail and press it against the rail until you hear the clip snap into place. See the figures below.

Size 1 (TPRPM009) and Size 2 (TPRPM038) Power Interface Modules (mm/in.)

Size 3 Power Interface Module (TPRPM080) (mm/in.)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?