DOCA0270EN-02

Power Devices

TeSys island offers two types of power devices:

  • Standard and SIL* starters that include a contactor and provide the following functionality as part of a TeSys avatar:

    • Load control management

    • Electrical protection functions

    • Digital asset management

  • Power interface modules that monitor current but do not provide load control. Load control must be provided by a downstream external power device like a solid-state relay or a soft starter.

Avatars that include power devices can provide load level energy monitoring when a voltage interface module (VIM) is installed in the TeSys island .

SIL starters in combination with a SIL interface module (SIM) can achieve certified Stop Category 0 and Stop Category 1 functions. *

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?