SIL Starters
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
For complete instructions about functional safety, refer
to the TeSys™ island Functional Safety Guide, 8536IB1904.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
SIL* starters provide similar functions to standard starters but are associated with a SIL interface module.
The main functions of the SIL starters are as follows:
-
Provide Stop Category 0 and Stop Category 1* functionality
-
Provide operational control for loads
-
Measure electrical data related to the load
-
Provide energy monitoring data when a voltage interface module is installed in the TeSys island
Multiple SIL starters might be needed for a single TeSys avatar function. For example, the avatar Motor Two Directions - SIL Stop, W. Cat 1/2* includes two SIL starters. In addition, avatars using SIL starters always include a SIL interface module.
The SIL starters are connected:
-
Upstream to a circuit breaker
-
Downstream to the load
The SIL starters communicate with the bus coupler, sending operational data and receiving commands.
SIL Starter Ratings
|
Power Ratings |
Amperage |
Reference |
|
|---|---|---|---|
|
kW |
hp |
||
|
4 |
5 |
0.18–9 |
TPRSS009 |
|
11 |
15 |
0.5–25 |
TPRSS025 |
|
18.5 |
20 |
0.76–38 |
TPRSS038 |
|
30 |
40 |
3.25–65 |
TPRSS065 |
|
37 |
40 |
4–80 |
TPRSS080 |
WARNING