DOCA0270EN-02

Wiring Precautions

Read and understand the following precautions before performing any procedures in this guide.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside this equipment.
  • Use only the specified voltage when operating this equipment and any associated products.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Use appropriate interlocks where personnel and/or equipment hazards exist.
  • Power line circuits must be wired and protected in compliance with local and national regulatory requirements.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices per local and national regulatory requirements.
Failure to follow these instructions will result in death or serious injury.
WARNING
Fire
  • Use only the specified wiring gauge range with the equipment and comply with the specified wire termination requirements.
  • Tighten the power line connections to the specified torque values.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
Unintended equipment operation
  • Use shielded cable for all communication wiring and when specified.
  • Always route communication wiring and power wiring separately.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?