DOCA0270EN-02

Long Start

The Long Start function detects when a motor remains in the Start state for an excessive period of time.

If enabled, this protection function triggers a Long Start trip when the motor is in the Start state, and one of the following conditions occur during the specified Long Start Trip Delay:

  • Average current too low: the average current remains below the specified Long Start Trip Level

  • Average current too high: the average current rises above the specified Long Start Trip Level but does not fall below it again.

Long Start Trip

I1

Phase 1 Current

I2

Phase 2 Current

I3

Phase 3 Current

T

Long Start Trip Delay

A

Iavg

B

Iavg ≥ 30%

C

Iavg ≤ Long Start Trip Level

D

Iavg ≥ Long Start Trip Level

E

# of Crossings = 1

F

Long Start Trip

NOTE: Number of Crossings = the number of times the value of current crossed (from above to below, or below to above) the Long Start Trip Level.

Average Current Continuously Exceeds the Long Start Trip Level (1 Crossing)

G

Long Start Trip Level

H

Long Start Trip Delay (in Start State)

I

Current

Ir

Rated Current

t

Time

   

Average Current Does Not Reach the Long Start Trip Level

G

Long Start Trip Level

H

Long Start Trip Delay (in Start State)

I

Current

Ir

Rated Current

J

Run State

t

Time

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?