DOCA0270EN-02

Island View Panel

The Island View panel displays status information for each device on the island.

  • By clicking on a graphical representation of the device, you can obtain status information, including asset data and product identification.

  • With the appropriate permissions, you can use Test mode.

Click the Island View panel to view a graphical representation of the island. The status of each device is displayed above the device on the island. A green circle with a check indicates that the device is in the ready state. A red alert symbol indicates that there is a device event on that physical device.

Island View

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?