OMT IPv6 Connection
Use this procedure to connect to TeSys island with the Operation and Maintenance Tool (OMT) after the island has been physically installed and powered up. The OMT will connect directly to the bus coupler using the default IPv6 address.
To perform this procedure, the island must be on the network and able to communicate with the OMT using a wireless or wired connection on a standard Windows® operating system.
Connecting to the TeSys island with the OMT via IPv6
| Step | Action |
|
1 |
Verify that your PC is connected to the same network as the bus coupler through a wireless or wired connection. |
|
2 |
Access the Network tab on your PC using File Explorer. |
|
3 |
Under Other Devices, the TeSys island will appear as "TeSysisland_FFFF." If the TeSys island does not appear, you may have to disable the firewall running on your PC. |
|
4 |
Right click on "TeSysisland_FFFF" and select Properties. The properties for the TeSys island will be displayed. |
|
5 |
Click the Device web page link. This is the IPv6 IP address of the bus coupler. The OMT will launch in your default browser. |
|
6 |
If you are taken to the page, "Your Connection is not private":
|
|
7 |
Login with the default username and password (admin, schneider18) and click Login. |
|
8 |
The Change Password window will open. Set a secure password and record it before continuing. If you forget your password, a factory reset will be required to regain access to the OMT. You are now logged into the OMT and connected to the TeSys island . |