I/O Module Wiring
Use the following guidelines and refer to the TeSys Avatar wiring diagrams to wire the I/O modules.
-
Remove the spring terminal connector. It is positioned on the top of the module, behind the flat cable connection.
-
Refer to the table and figures below and make the power and control connections. See Accessories Cabling for cable types and sizes.
-
Insert the spring terminal connector back into the top of the module.
Pin | Digital I/O Module | Terminal Identification | Analog I/O Module | Terminal Identification |
---|---|---|---|---|
1 (closest to DIN rail) |
Input 0 | I0 | Input 0 + | I0+ |
2 | Input 1 | I1 | Input 0 – | I0– |
3 | Input Common | IC | NC 0 | NC0 |
4 | Input 2 | I2 | Input 1+ | I1+ |
5 | Input 3 | I3 | Input 1 – | I1– |
6 | Output 0 | Q0 | NC 1 | NC1 |
7 | Output Common | QC | Output + | O+ |
8 (closest to front face) |
Output 1 | Q1 | Output – | O– |