DOCA0270EN-02

Connecting to the OMT Using the Default IP Address

Connect to the island with the Operation and Maintenance Tool (OMT) using the IPv6 or default IPv4 address.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?