Stall
The Stall function detects high current intensity, typically associated with a locked or stalled motor, while in the Start state.
If enabled, this protection function triggers a Stall trip when the motor is in the Start state, and the maximum phase current exceeds the specified Stall Trip Level for a time longer than the specified Stall Trip Delay.
This function is typically enabled in addition to the Long Start protection function, setting a higher acceptable current intensity level and a shorter trip delay.
Stall Trip Versus Long Start Trip
|
D |
Stall Trip |
E |
Stall Level |
|
F |
Long Start Trip Level |
G |
Long Start Trip Delay |
|
I |
Current |
Ir |
Rated Current |
|
t |
Time |
T |
Stall Trip Delay |