Standard Starters
Standard starters provide load control, electrical and thermal protection functions, and digital asset management.
Starters provide the following main functions:
-
On/Off power control for loads (three phase or single phase)
-
Electrical data measurement related to the load
-
Energy monitoring when a voltage interface module is installed on the TeSys island
-
Functional testing and simulation
-
Event logging and counters
Multiple starters might be needed for a single TeSys avatar function. For example, a motor two-direction avatar includes two standard starters.
The standard starters are connected:
-
Upstream to a circuit breaker
-
Downstream to the load (three phase or single phase)
The starters communicate with the bus coupler, sending operational data and receiving commands.
Standard Starter Ratings
|
Power Ratings |
Amperage |
Reference |
|
|---|---|---|---|
|
kW |
hp |
||
|
4 |
5 |
0.18–9 |
TPRST009 |
|
11 |
15 |
0.5–25 |
TPRST025 |
|
18.5 |
20 |
0.76–38 |
TPRST038 |
|
30 |
40 |
3.25–65 |
TPRST065 |
|
37 |
40 |
4–80 |
TPRST080 |