Enclosure Requirements
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
Unintended equipment operation
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
TeSys island modules are designed as Zone B, Class A industrial equipment according to IEC/CISPR Publication 11. If they are used in environments other than those described in the standard, or in environments that do not meet the specifications in this guide, they may not meet electromagnetic compatibility requirements in the presence of conducted and/or radiated interference.
All TeSys island modules meet European Community (CE) requirements for open equipment as defined by EN61131-2, and as open equipment per the North American standards. You must install them in an enclosure designed to meet the specific environmental conditions of the installation and to minimize the possibility of personnel unintentionally contacting hazardous voltages. The enclosure should be constructed of metal to improve the electromagnetic immunity of the TeSys island and should have a keyed locking mechanism to minimize unauthorized access.
DANGER
WARNING