DOCA0270EN-02

Motor Two Speeds Two Directions - SIL Stop, W. Cat 3/4

NOTE: Safety Integrity Level according to standard IEC 61508. Wiring Category 3 and Category 4 according to ISO 13849.

Low Speed Wiring

Accessories

Legend

A Mechanical interlock
B Parallel link
C Reversing link
F Forward starter
R Reverse starter
LS Low speed
HS High Speed
SS-1 SIL starter 1
SS-2 SIL starter 2
SS-3 SIL starter 3
SS-4 SIL starter 4

High Speed Wiring

Accessories

Legend

A Mechanical interlock
B Parallel link
C Reversing link
F Forward starter
R Reverse starter
LS Low speed
HS High Speed
SS-1 SIL starter 1
SS-2 SIL starter 2
SS-3 SIL starter 3
SS-4 SIL starter 4

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?