DOCA0270EN-02

Switch Off Island

Issue the Switch Off Island command to turn off all loads on the TeSys island , so the system can be used for maintenance purposes.

  1. Click the Control Panel icon.

  2. Click Switch Off Island.

The TeSys island is placed into a minor event state. The red MS LED illuminates on the bus coupler (TPRBCEIP only). All outputs on the island are opened. The connection to the PLC remains in place. The OMT connection also remains active.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?