System Event Log Attributes
System Event Log attributes are defined in the following table.
|
Attribute |
Description |
|---|---|
|
timestamp |
The system time YYYY-MM-DDThh:mm:ss.mmm Example: 2018-01-02T15:02:59.970 |
|
avatarName |
The user defined avatar name |
|
avatarNumber |
The number of the avatar in the digital tool |
|
avatarSILGroup |
The SIL* group of the avatar |
|
deviceTag |
The user defined device tag |
|
deviceNumber |
The number of the device in the physical order of the system (the Node ID on the internal bus) |
|
value |
The new value of the data change event being logged. |