DOCA0270EN-02

Energy Monitoring

The Time of Use window provides graphs showing the accumulated energy during the time each channel is enabled. Channels can be enabled or disabled via the Time of Use configuration window in the OMT or via the PLC. The four channels are independent of each other. The Time of Use configuration window in the OMT also allows you to preset energy data in these graphs.

System Energy Monitoring

Time of Use

To access the settings in the Time of Use window for the avatar:

  1. Click the wheel symbol in the top right corner to display the settings.

  2. Change the values and click Set.

  3. Close the window.

Active and Reactive Energy

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?