DOCA0270EN-02

Installing the Micro SD Card

To install the SD card:

  1. Insert the SD card into the bus coupler’s card slot.

  2. Push until you hear it “click.”

Installing the SD Card

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?