DOCA0265EN-07

Monitoring the Communicating Voltage Releases

Presentation

The voltage releases undergo wear due to the number of opening/closing operations. It is recommended to check them at periodic intervals to decide whether they must be changed or not.

In order to assist with the maintenance of the communicating voltage releases the MicroLogic Active control unit monitors:

  • The diagnostic and communicating MX1 opening voltage release (MX1 diag&com).

  • The diagnostic and communicating XF closing voltage release (XF diag&com).

For more information about the maintenance of voltage releases, refer to DOCA0305•• MasterPacT MTZ IEC Circuit Breakers with MicroLogic Active Control Unit - Maintenance Guide.

Prerequisites

The prerequisites for monitoring the MX1 and XF communicating voltage releases are the same as the prerequisites for using the ULP wired communication.

Operating Principle

The MicroLogic Active control unit:

  • Checks the presence of voltage releases.

  • Counts the number of operations performed by the voltage releases.

  • Monitors the state of the internal circuit of the voltage releases.

  • Generates events when it detects incorrect operation of the voltage releases or cannot detect the presence of the voltage releases.

Data Availability

The communicating voltage release operation counters are available on a server or remote controller using the wired communication network.

Predefined Events

The monitoring of the communication voltage releases generates the following events:

Code

Event

History

Severity

0x1460 (5216)

Invalid self test - MX1 voltage release

Diagnostic

Medium

0x1461 (5217)

MX voltage release not detected

Diagnostic

Medium

0x1462 (5218)

Invalid self test - XF voltage release

Diagnostic

Medium

0x1463 (5219)

XF voltage release not detected

Diagnostic

Medium

Recommended Actions

Code

Event

Recommended actions

0x1460 (5216)

Invalid self test - MX1 voltage release

Plan to replace the MX1 voltage release.

0x1461 (5217)

MX voltage release not detected

Check the connection of the MX voltage release.

0x1462 (5218)

Invalid self test - XF voltage release

Plan to replace the XF voltage release.

0x1463 (5219)

XF voltage release not detected

Check the connection of the XF voltage release.

Contact Schneider Electric Support or your Schneider Electric Services representative for more information about who can carry out the recommended actions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.