DOCA0265EN-07

Reboot or Restart MicroLogic Active Control Unit

Reboot MicroLogic Active Control Unit

Events which require a reboot of the MicroLogic Active control unit are:

Reboot the MicroLogic Active control unit by simultaneously pressing the 5 buttons , OK, Back, Up, and Down.

IMPORTANT: The standard protection functions remain active during the reboot process.

Restart MicroLogic Active Control Unit

Restart of the MicroLogic Active control unit is required when:

  • The rated frequency setting is changed (MicroLogic Active E/EP/Ei control unit only)

  • The MicroLogic Active HMI does not display protection alarms or measures screens

  • The MicroLogic Active loses the Zigbee signal

Restart the MicroLogic Active control unit in one of the following ways:

  • Switch off the power supply to the MicroLogic Active control unit, and switch it back on.

  • Click the Restart Module button on the Launch Firmware Upgrade page of EcoStruxure Power Commission software.

The settings of the MicroLogic Active control unit are not affected by the restart.

IMPORTANT: The standard protection functions remain active during the restart.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.