DOCA0265EN-07

Closing Function

Presentation

MicroLogic Active control units receive and process electrical closing orders. An event is generated on closure.

Operating Principle

Closing orders can be sent as follows:

  • Directly through a mechanical closing pushbutton.

  • Locally through an external opening pushbutton, connected directly or via the BCIM module to the XF communicating closing voltage release

  • Remotely through a remote order which is managed by the MicroLogic Active control unit.

Opening orders have priority over closing orders. No closing orders are taken into account as long as an open order is active.

Management of Closing Function

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Do not operate the circuit breaker without confirming that doing so will not create a hazardous situation.
  • Do not allow any person to work on the electrical network without physically validating the successful execution of the local or remote software actions for closing the circuit breaker or switching on the electrical circuit.
Failure to follow these instructions will result in death or serious injury.
WARNING
HAZARD OF CLOSING ON ELECTRICAL FAULT
Do not close the circuit breaker again without first inspecting and, if necessary, repairing the downstream electrical equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The MicroLogic Active control unit manages closing orders issued by the following means:

The control logic for managing closing orders is summarized in the following graphic and table:

CB opened

Circuit breaker is open

Auto Local

Control mode is Auto Local

XF control by BCIM enabled

Control of the XF voltage release by the BCIM module is enabled.

BCIM IO mode=Open/Close

The BCIM IO mode parameter is set to Open/Close.

BCIM IO close

Close order from the closing pushbutton connected to the BCIM module

FDM121 close

Close order from FDM121 display

Auto Remote

Control mode is Auto Remote

COM close

Close order from a server or remote controller

Webpage close

Close order from IFE/EIFE webpage

Close

MicroLogic Active close order to the XF communicating closing voltage release

Predefined Events

The function generates the following predefined events:

Code

Event

History

Severity

0x1001 (4097)

Circuit breaker closed

Operation

Low

0x0411 (1041)

Closing order sent to XF voltage release

Operation

Low

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.